Dear Technical support,
I am using a TI FDC1004EVM Evaluation Module to measure the level of water as it passes through a restrictive channel in a device and then exits. The level readings seem to be very accurate, however I am struggling to calculate the total volume of water that has passed through the device. The Sensing Solutions EVM GUI allows me to output the readings to Excel, where I am able to calculate the liquid level at each time interval (knowing the volume of the channel the liquid is passing through, the capacitance of the vessel when empty and the capacitance of the vessel when full of water). I need to use this information to calculate the total volume of liquid that has passed through the vessel. How could I go about this?
Many thanks in advance,
David