Hi,
In mmWave Sensing estimator, I am trying to use IWR1443 in long range mode. I have the following observations:
1. It does not consider Simultaneous Transmit mode in the TX
2. It doesnot consider only real data to be captured by ADC.
I am considered about these, because, if I consider these my sampling rate is better, and I can achieve large range, range resolution and max velocity.
My question is , whether these two observations are true??
and whether my assumption that if I consider them I can get larger range and velocity??
Thanks in Advance,
Santhana Raj
[unlocked 1/19/18>LE