This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDC1000-TDC7200EVM
Can the TDC1000-7200 EVM tested without transducers and using function generator or alternatives. This way I can have flexibility on the signal going in RX path and later choose transducers accordingly. Is this a valid idea?
Hello,
Thank you for the immediate support. I think its better to input directly at RX so I need not give a bias.
I have a doubt, what specification of function generator will do the job. My transducers are sending at 1MHz for water flow measurement in pipes.
Regards,
Prudhvi Sagar