This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: clock/sync pins for cascading

Part Number: AWR1243

We are planning to cascade four AWR1243 devices using a single master, and are looking to utilize the two 20GHz output signals.  For the FMCW_CLKOUT and FMCW_SYNCOUT outputs, how closely matched in phase are they at the device pins?  Is there an internal phase adjustment for one or both of the outputs in order to calibrate and match them in case there may be part to part and/or possible variances over temperature?.  Also, I've seen some differing information on the input buffer sensitivity.  One response from TI states the input should be 0dBm, another says that the buffer sensitivity is -10dBm.  Please confirm what the acceptable range is.  I came across +6dBm output power in one post, and +7dBm in another, but obviously verifying this is not as much of a concern for me.  Thanks -

  • Hi,

    We are checking the design reference we are working and will get back to you later today

    thank you
    Cesar
  • Hi Victor,

    Regarding the input power requirements for the FMCW_SYNCIN pins, the Cascade Radar application note is the definitive guide for now www.ti.com/.../swra574a.pdf. TI is specifying this system implicitly by way of the example link budget shown in Figure 7. The values of 0.1dBm to 1.3dBm shown at the FMCW_SYNCIN are the resulting input power range we expect based on our link budget shown. That is all we are specifying at the moment.

    Regarding your phase adjustment question I will get back to you after discussing this with my team. It may take a few days to get back to you.

    Thank you,
    Randy
  • Hi Victor,

    Just confirmed today, there is no internal LO alignment mechanism. There is very minimal delay mismatch between the FMCW_SYNCOUT and FMCW_CLKOUT pins. All delay match must be provided by the PCB. Recommendation is to match to whatever your minimum PCB fabrication tolerances can allow. Better match ensure better phase alignment between the devices which would then need to be calibrated out with the phase-shifters along the TX paths.

    Please let me know if that answers all of your questions on this topic.

    Thank you,
    Randy