This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Regarding the linked post it was mentioned that there it will be worked on a Python script to parse the data from the mmWave Demo coming from the UART.
Is this already published? I did not fin one.
I need it to for the data of the two heatmaps that are created during the demo.
Kind regards,
Max
Hello Max,
There is not a public Python script to parse the data. However, please refer to the attached slide deck for data structure information. Additionally, this version of the Demo Visualizer enables logging of the output to a CSV file.
If there are additional questions please let me know.
- Amanda