This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7201EVM and MSP430Launchpad



The application we intend to use this device is a bit different than TOF. Basically we need the time between Start and Stop signal. I have 2 questions for you

    1. Will there be a problem if the frequency of the start is 50KHz. (for our application we need 50 KHz)

I see 100ms sampling and that would not work with our 50KHz START frequency 

https://e2e.ti.com/support/sensor/ultrasonic/f/991/t/604141

 

If this is the limitation of the TI launchPAD, can we do anything to overcome this by just using OTS boards.

 

    1. Is there any limitation differences between mode 1 and mode 2?    Will the resolution stay the same (55ps)?

 

Regards,