Other Parts Discussed in Thread: , AWR1642BOOST, AWR1443BOOST
Hi ,
I have four question,please help.
Q1.Traffic Monitoring Demo must use IWR1642 ES2.0 , I can't see white sticker that says "ES2.0" in my EVM board ,So the IWR1642BOOST is ES1.0?
I have four question,please help.
Q1.Traffic Monitoring Demo must use IWR1642 ES2.0 , I can't see white sticker that says "ES2.0" in my EVM board ,So the IWR1642BOOST is ES1.0?
Q2.What different with the ES1.0 and ES2.0 (performance or ) ?
Q3.www.ti.com/.../IWR1642BOOST
the link is ES1.0 or ES2.0
Q4.about People Counting Demo , I have experment some config , the max distance is 14m , do your team have try more then 14m config file (20m?40m?).
Thanks
/Melvin