This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP102: The time required for the TMP102 to boot up

Part Number: TMP102


Dear Sir/Ms.

Because some parameters of the customer need to be set according to the temperature that the thermal sensor reads, and as soon as possible, the better,

Now that the SoC starts reading data from the thermal sensor after power on, it reads a value of 0 degrees from the beginning and reads the correct value after some time.

Because we applied at -40~85 degrees, so at the beginning of reading 0 degrees, FW can not determine whether it is correct

So I want to ask the following questions

1. TMP102 "How long after power on" can read the first correct temperature data
2. Is there any register that confirms that the thermal sensor is ready?

Best Regards,

Kami Huang