Other Parts Discussed in Thread: UNIFLASH,
Hello,
Occupancy detection demo does not run normally.
Board: AWR1642BOOST, Com port is properly set, the right image is flashed by uniflash, Windows 10 PC, other demos like people count is working well...
Is there any way to fix this issue?
Here is a copy of DOS prompt when I ran the demo:
=====
C:\ti\mmwave_automotive_toolbox_2_0_0\labs\lab0003_occupancy_detection\gui>od_demo.exe 13 12 C:\ti\mmwave_automotive_toolbox_2_0_0\labs\lab0003_occupancy_detection\chirp_configs\od_demo_car_0318_1p0.cfg 1 0
Starting UI for Occupancy Detection Demo ....
Opening configuration file C:\ti\mmwave_automotive_toolbox_2_0_0\labs\lab0003_occupancy_detection\chirp_configs\od_demo_car_0318_1p0.cfg ...
comportnum_str =
'COM13'
comportnum_str =
'COM12'
Sending configuration to XWR1xxx C:\ti\mmwave_automotive_toolbox_2_0_0\labs\lab0003_occupancy_detection\chirp_configs\od_demo_car_0318_1p0.cfg ...
sensorStop
Done
flushCfg
Done
dfeDataOutputMode 1
Done
channelCfg 15 3 0
Done
adcCfg 2 1
Done
adcbufCfg -1 0 0 1 1
Done
profileCfg 0 77 250 10 40 0 0 98 1 64 2200 0 0 40
Done
chirpCfg 0 0 0 0 0 0 0 1
Done
chirpCfg 1 1 0 0 0 0 0 2
Done
chirpCfg 2 2 0 0 0 0 0 1
Done
chirpCfg 3 3 0 0 0 0 0 2
Done
frameCfg 0 3 128 0 160 1 0
Done
lowPower 0 1
Done
guiMonitor -1 0 1 1
Done
calibDcRangeSig -1 0 -5 8 256
Done
zoneDef 2 13 16 9 15 13 16 27 15
Done
coeffMatrixRow 0 -14.409613 -8.187467 -8.019457 3.833826 4.045485 -0.539210
Done
coeffMatrixRow 1 -12.465002 -2.228748 -5.612140 4.324446 -7.912656 0.528747
Done
coeffMatrixRow 2 -9.210626 -3.004206 -0.082298 -2.949700 7.538751 0.246658
Done
coeffMatrixRow 3 -1.917373 2.299849 2.389683 7.035545 6.675194 -0.099186
Done
meanVector 23.992751 23.689970 -3.388539 -3.691319 0.816150
Done
stdVector 8.495360 8.497394 2.198640 2.432388 0.196337
Done
oddemoParms 12 0.001
Done
sensorStart
Error -1
=====
I tried all chirp config files: od_demo_car_0318_1p0.cfg, od_demo_car_0318_3p0.cfg and od_demo_carseats_0302_3p0.cfg but results are same. Only see blank gui display.
Best Regards,
Katsuhiro