Other Parts Discussed in Thread: IWR1642
Hi,
When using the DCA1000EVM the quick start guide only refers to using mmwave studio. If I want to configure the EVM with some given parameters and then stream the data out continuously I have the following questions:
- With the out of the box demos is it only the "Capture Demo" that can easily be configured to stream out data over LVDS?
- The capture demo docs in the mmwave_sdk_user_guide state "this demo (when configured for streaming) needs mmWave sensor device to be interfaced with another device that has a compatible LVDS/CSI2 interface. For this purpose is the DCA1000EVM a compatible device?
- In section 6 of the mmwave_sdk_user guide "Streaming over LVDS" it talks about three modes of operation (MSS only option, DSS only, and MSS and DSS running in coperative mode). I can't find a description of these modes. Which one should I go for - ideally I want to stream data continuously for as long as possible so that the receiving computer will just drop frames if it can't handle the rate.
Is there a better way than trying to use the capture demo? If there is a how to guide that would be great.
Thanks