This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
we try to test the can bus of AWR1642 boost.
However the "selection 4: TX/Rx" does not work well.
It has always error in transit and receive.
Could you test this unit and solve this problem?
We have check the board, and put the 0 ohm resistor on the board.
Thanks,
Kang
Hi Kevin,
the circuit is checked as you said. however, we can still run the test cases of first three.
the 4th selection has not yet run correctly.
Could you see whether the CAN driver for AR1642 boost is not tested?
As I knew, AR1443 has the same problem before.
Thanks,
Kang
Hi Kang,
This issue seems to be similar to the problem discussed in the following thread. As defined here, could you please check if there's activity on the CAN bus using an oscilloscope?
CCS/AWR1642BOOST: CAN Unit Test Error
Thanks
-Nitin
Hallo Nithin,
we havenot seen any signal from the CAN bus.
So I just doubt that the CAN driver test program in mode 4 does not work correctly.
Could anyone from TI help?
Thanks,
Kang
Hello Kang,
Please refer to the “Appendix A.4” in this App Note for the “ECO’s on AWR1642BOOST” for external Tx/Rx to be functional.
Thanks,
Raghu