Hi,
I'm reading Image Creator User Guide and need to clarify the header length and the word "size".
RPRC format has RPRC header and Section Headers.
Q1: Are those headers always 24 bytes long?
Q2: In the section header, there is "Section size". Does this value indicate the exact data length?
For instance, if the value of section size is 0x3C (60), then is the length of the section data after the section header 60 bytes?
Best Regards,
-Kevin