Other Parts Discussed in Thread: DCA1000EVM, , AWR1443
Hello,
I am currently working with a DCA1000EVM connected to an AWR1443BOOST radar. The assembly is setup as instructed in the DCA1000EVM Quick Start Guide: 2 power supplies (5V, 2.5 A), 2 micro USB cables, 1 Ethernet cable, booted in SOP Mode 2.
I am having issues with running the DataCaptureDemo_xWR.lua Script in mmWave Studio as is instructed in the DCA1000EVM Quick Start Guide. I am able to issue a board reset, to connect the RS232 COM port and, after hitting run with DataCaptureDemo_xWR.lua Script selected, to successfully load BSS FW and MSS FW onto the device. SPI is then successfully connected and RF is powered-up without issue. After this, however, I receive a pop-up error saying "No Frame config information" along with a RadarStudio PostProcessing pop-up displaying no data.
How do I correct this issue of "No Frame config information", ensure that I am indeed collecting data, and display the data collected in the PostProcessing window?
Thanks,
Khalid