This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: How to create config files for chirp params in mmW sensor demos, e.g., people counting

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: MMWAVE-SDK

I'm using the IWR1642BOOST ES2.0,  Industrial Toolbox 2.5.0, mmW Sensing Estimator 1.2.0, mmW Demo Visualizer 2.0.0, and CCS 8.1.0.  Windows 10 OS.

The people counting demo seems to work fine by flashing the binaries and through CCS Debug mode. 

In the setup window of the people counting demo, there is an option to Load Chirp Config, as well as other demo specific parameters.  

1) How do I create my own chirp configuration files? mmW Sensing Estimator creates a .json file, but this does not seem to be the correct format expected by the demo.

2) If the mmW Sensing Estimator does not save appropriate .cfg files for chirp configuration, what is the intended workflow for that tool?  how do i make use of that .json file it creates?

3) The mmW Demo Visualizer does make a .cfg file that appears to the correct format, but also includes other demo specific parameters which i assume would not be appropriate for other demos. Is Demo Visualizer usable for other demos?

Sorry for all the noob questions.  I'm new to the TI tools and haven't done any serious hands-on HW work in a while, so please don't skip any details :).

Thanks

  • Hi Philip,

    Chirp parameters and format are explained the mmWave-SDK User Guide on page 14. If you have questions on specific parameters just let us know!

    You can only extrapolate FrameCfg and ProfileCfg from the Sensing Estimator at this time.

    Lastly, the visualizer is only for the standard SDK demo and is intended to provide an out-of-box experience. The other demos on the TI-Resource Explorer have their own GUI's in order to demonstrate the sensor's capability for a particular application.

    If you have any more questions then let us know!


    Cheers,
    Akash