Hi,
I came from here;
It seems like the following Flash has been verified for IWR1642, but is this till true for ES2.0 device ?
• MX25U1633FZNQ - 16Mb, 1.65V - 2.0V, WSoN(6x5mm), -40 to +125 Degree Celsius
• MX25V1635FZNQ - 16Mb, 2.30V - 3.6V, WSoN(6x5mm), -40 to +125 Degree Celsius
• MX25V8035FM1Q - 8Mb / 2.30V - 3.60V / Quad SPI (104MHz) / 8 SoP / -40°C to 125°C
Best Regards,
NK