Other Parts Discussed in Thread: AWR1642, IWR1642
I asked a question a while back here: https://e2e.ti.com/support/sensor/mmwave_sensors/f/1023/t/706450
This time, after hitting the Connect button on mmWave-Studio to connect to the RS-232 port, I load the firmware using the two "Load" buttons. Then I click on the "SPI Connect" button in order to connect to the SPI port. Just like the earlier issue, nothing happens here.
I don't understand the problem this time. My AWR1642 is correctly set to development mode by shorting SOP0 and SOP1, the TSW1400, AWR1642 and MMWAVE-DEVPACK are connected to my Windows virtual machine.
My AWR1642 has been flashed with mmWave Demo software. Any help is greatly appreciated!
Regards,
Raashid