Part Number: TDC1000-TDC7200EVM
Hello, I am using TDC1000 TDC7200 EVM for non invasive level measurement.
It works fine with GUI for level below 10-12 CM, but once i increase the level GUI shows some random readings.
I have updated EVM with latest firmware, i.e. TDC1000_7200_FW-v2.01-1MHz file.
Is there any limitation in GUI for level measurement ? What are the settings to measure the level up to 2-3 meters.
Thanks.!