This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI-RTOS
Even though the maximum IF bandwidth for the receiver is 5MHz would it break Nyquist convention to sample anything above 3.125MHz in the complex case since the maximum sample rate of the ADC for a complex signal is 6.25MHz? If so, would the purpose of designing a receiver with 5MHz IF bandwidth be for sampling only the real component of a signal?