Other Parts Discussed in Thread: AWR1642
Tool/software: TI-RTOS
If the maximum sampling rate of the ADC on the AWR1642 for complex data is 6.25 Msps, then this means that the sampling rate of real data is 3.125 Msps and the sampling rate of imaginary data is 3.125 Msps. Are you already taking Nyquist into account here or is the maximum frequency of the signal that can be accurately sampled half of the sampling rate for real and imaginary - 1.5625 MHz? If this is true, then how am I supposed to utilize the full 3MHz bandwidth of the ADC?