This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Changing IP/ MAC address at DCA1000EVM

Part Number: DCA1000EVM


Hello,

I also need to change the IP and MAC address of DCA1000EVM, the user guide says that I need to update EEPROM using the command CONFIG_EEPROM_CMD_CODE, but it doesn't describe the data format of this command. Could you please give me some information about this?

Yours Sincerely,

Zhiyang

  • Hello Zhiyang,
    Presently we do no have a platform /SW for you to directly issue the commands to the DCA1000. Do you have in mind to develop your own environment to do that if the DLL details were available?

    Regards,
    Vivek
  • Hello Vivek,

    Thanks for the reply.

    I do not develop my own environment, the command CONFIG_EEPROM_CMD_CODE is one of the command codes already provided in the protocol between the computer and DCA1000EVM, and is described in the DCA1000EVM user guide. The command is issued through UDP protocol. However, the user guide doesn't provide the data format of this command code. I think I need to know the data format if I want to use this command code to change the IP address of DCA1000EVM.

    Yours Sincerely,

    Zhiyang

  • Hello Zhiyang,
    This API is not available from mmwave studio tool today.

    Regards,
    Vivek

  • Hello Zhiyang,
    Unfortunately we do not have the SW tool to allow you to change the IP address. You would have to use the default IP address.

    Regards,
    Vivek