This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: IWR1642BOOST

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642,

As required, I load xwr16xx_mmw_demo.bin to IWR1642 EVM from mmwave_sdk_02_01_00_04.

then I conncet mmw demo visualizer(2.0) to EVM(IWR1642boost),and it shows COM15:115200 COM14:921600 waiting for data.....until I press the reset button on EVM.

then it shows  hardware connected.and i click the buttom of send config to mmwave device.but the console message tab return nothing.

whar should i do with this situation?

  • Hello Chao,

    This ticket will cover response for previous ticket you have filed for similar issue  : IWR1642BOOST: IWR1642BOOST

    Based on your GUI snapshot it seems like the device is responding and images loaded on device seem to be working well.

    Code running on device doesn't seem to like the configuration you are sending via the visualizer gui.  In order to make sure it is the configuration and not something else that is creating this error, can you please try loading the configurations provided in demo directory or SDK's OUt of box demo.

    Typically these are .cfg file and can be send to the device via load .cfg option on visualizer's tab which shows the plots. Please let us  know how that works.

    Thank you,

    Vaibhav

  • Hi,this problem has been solved.the version of the chip is es1.0 ,But the version of SDK is 2.0 or 2.1.

    when i use the sdk(v1.2),then It's working  normally ^.^