Other Parts Discussed in Thread: LMP91300, LDC1612, LDC1312, LDC2112
Hi, I am looking to use LDC0851 to sense a metal target through a metal membrane. The coils will be inside a metal enclosure pressed up against a 0.006" thin metal face as part of the enclosure. I am using 2 separate PCB coils (identical design from the same manufacturing lot), one for the sense and one for the reference. To try and keep the coils matched due to one having a constant metal "bias", I have placed the same thin metal piece against the reference coil. I cannot get the outputs to switch when a metal target approaches the sense coil.
Theoretically the inductances should be matched since the sense and the reference see the same bias. I have confirmed that the LC tank frequency with this configuration is within the datasheet operating conditions. I am unsure if there is enough inductance change when trying to sense a metal target through this metal face that would cause the output to switch. Has this chip been used in this type of configuration before? I am interested in this chip because it is purely analog with little temperature dependence due to the dual coil design. The metal face I am referring to is something like the below.