Dear AWR1243 Experts,
I developed AWR1243 cascaded device with ES2.0 and I had simple tests with devices.
Recently, I read a post about power degradation issue at cascaded device. (the related question)
It seems that this problem is very critical for my system because I'm planning to gather precise radar data.
I had to post this question because I don't have enough facility to evaluate current system as TI has.
Referring to Vivek's answer to previous post, I have some questions as below.
1. Just to clarify once again, is this problem happening for "master device" or "all master & slave devices"?
I wonder if the 20GHz SYNCIN pin is problem, maybe all other devices can be affected in cascaded configuration.
Or it may be limited to master device because it is only device that generates and feeded back LO signal.
1-a. Can we workaround this by not using transmiters of master device? (Using master device as receiver with giving up 3 Tx...)
1-b. Is it possible to share your test results in this forum? or do I need NDA to see results?
1-c. Is this power degradation happening when
a. 20GHz Sync is distributed via both FM_CW_SYNCOUT and FM_CW_CLKOUT
b. when using one of FM_CW_SYNCOUT or FM_CW_CLKOUT
also, when 20GHz signal is looped back to master and fed to
c. any pin between FM_CW_SYNCIN1 or FM_CW_SYNCIN2
d. or specific one pin FM_CW_SYNCIN1 or 2
1-d. Is it possible to compensate the power degradation of 20GHz signal to master device, by using some amplifiers in LO distribution circuit?
1-e. Regardless of Tx power backoff that I set, it seems that it is not able to transmit constant power with AWR1243 ES2.0 cascaded device in 77-81 GHz?
2. To update cascaded device with ES3.0, Could you let me know how I can update the system? I can't find out any detail resources.
2-a. Is ES3.0 only available to NDA users for now?