HELLO. i am going to design a temprature sensor circuit to sense the environment tempature so i have choose these two types of LM35CZ/NOPB and LM35DZ/LFT1 .. The input voltage of these two types of the sensor is ranges from 4-30 volt so if i apply voltage 6 volt or 12 volt DC . so will it be effect the performance of the sensor i mean will reading will effected by these reason??