This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have two questions about DCA1000EVM. Hope you could help me figure them out.
1. Can the raw data be stored in the file(People set in 'mmwave studio') at the real time? Each time I want to read the data in this file, I need to press the 'Post Processing' button in 'Mmwave studio' firstly. Then I have to wait some time until the data has be copied to the file? The longer time I need to wait when the file is bigger.
So I am confused that if the data was stored in SSD after it went through the ethernet interface, and then it was copied to the file after the capturation process finished?
2. From some threads from the forrum, I know that the DCA1000EVM cannot capture data for a long time beacause 'mmwave studio' will triger 'time out' signal. I want to know why the 'mmwave studio 'has to trigger 'time out' and what is the maximun time to trigger 'time out'?
Thanks,
William