This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC1004: thickness between a sensor and its associated shield

Part Number: FDC1004

Team, 

My customer has a question concerning the thickness between a sensor and its associated shield when using the FDC1004.

 

From Application Report SNOA928A, Capacitive Proximity Sensing Using the FDC1004, Page 6:

The size of the shield and distance to the sensor electrode significantly affects the sensing range. A shield

that is larger than and closer to the sensor electrode reduces the sensitivity and maximum range, but it

limits the amount of interference seen by the sensor electrode. A smaller shield further away from the

sensor electrode has an opposite effect on sensitivity and detection range. For more information on

shielding effects, refer to the Capacitive Sensing: Ins and Outs of Active Shielding application note.

What is the tradeoff for the shield to sensor distance versus sensing range? While most of the application notes reference FR4 at a thickness of approximately 60 mils, Application Report SNOA926A uses Plexiglas at a thickness of approximately 23.6 mils. I’m primarily interested in thicknesses less than Plexiglas.?

Thank you for your help