This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I've connected my IWR1443BOOST pin 7 on J5 to CC3200 pin 39. I've been using a baud rate of 2000000 and I've been monitoring the serial output via energia's built-in serial monitor. No matter what I do, I can't send the information over. Any ideas
Hello,
You cannot use AR_BSS_LOGGER for this purpose, Even though its UART port it has different functionality.
Processed data would come through AR_MSS_LOGGER for this you need to modify EVM as instructed above.
To locate the resistors you could use the assembly diagram from the below link as well from the IWR1443BOOST product folder.
http://www.ti.com/lit/zip/sprr254
I have highlighted your region of interest with the blue color marking.
Thanks and regards,
CHETHAN KUMAR Y.B.