This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: PULL UP/PULL down resistors on PMIC question?

Part Number: IWR1443BOOST


From the specification of lp87524b/j, the pull up resistor for PGood, GPIO1, GPIO2, GPIO3 should be 10K ohms, why the EVM board use 4.99K ohms, Can we change to 10k ohms? The PMIC_NRST should use pull down resistors, why use pull up resistor, can we use pull down resistor for this?

Thanks,