This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443: FMCW radar angle resolution (MUSIC algorithm)

Part Number: AWR1443

I have read several TI training documents, and find that the angle resolution is determined by the number of receiving antenna.

The formula is :   angle resolution = 2 / N, and the doa algorithm is based on angle-FFT.

However, there's some subspace algorithms, such as , MUSIC ,ESPRIT, and they were called super-resolution algorithms.

Does this mean these super-resolution algorithms can  increase the angle resolution.

For example, if there is only 1 TX and 4 RX , in the angle-FFT, the resolution is 28.5deg. 

While I choose MUSIC algorithm , will the angle resolution increase? What is the formula? 

  • Hi

    The performance of MUSIC/ESPIRIT (when the number of targets is correctly estimated,) is bounded by the 'Cramer Rao Bound' (for high SNR scenarios).

    There is no closed-form expression for the 'Cramer Rao Bound' for multiple targets, however, it is fairly easy to calculate. You can use 'Fundamentals of Statistical Signal Processing: Estimation Theory (Kay, S. M.)' which has a section on how to calculate the bound for direction of arrival problems.

    In our experiments, MUSIC/ESPRIT has fairly good performance when the number of 'virtual antennas' is high (say 40). For small number of antennas (say 4) we haven't seen good performance.

    Regards
    Anil
  • Thanks, Anil

    I can not figure out the relationship between MUSIC angle resolution(two targets with same range and speed) and CRLB.

    Can you give me a brief introduction?

    The MUSIC method :

    Cramer Rao Bound: