Other Parts Discussed in Thread: UNIFLASH, , AWR1642
Dear TI:
my device is awr1642boost(5337900391) , uniflash 4.6.0.
1. the com port showed on PC is ok .
2. and I follow the sdk' demo(choose the com3, browse the demo's bin, put the sop0 and sop2, powered recycle with sw2), and uniflash the demo's bin successfully.
3. I follow the same steps in 2 above , of course i browsed the vital sign lab's bin, but it can not work.
[2019/2/19 下午12:35:35] [INFO] Cortex_R4_0: Initialization complete.
[2019/2/19 下午12:35:35] [INFO] Cortex_R4_0: Flashing process starting...
[2019/2/19 下午12:35:35] [INFO] Cortex_R4_0: Connecting to COM Port COM3...
[2019/2/19 下午12:35:35] [INFO] Cortex_R4_0: Reset connection to device
[2019/2/19 下午12:35:35] [INFO] Cortex_R4_0: Set break signal
[2019/2/19 下午12:35:55] [ERROR] Cortex_R4_0: Initial response from the device was not received. Please power cycle device before re-flashing.
[2019/2/19 下午12:35:55] [ERROR] Cortex_R4_0: Not able to connect to serial port. Recheck COM port selected and/or permissions.
[2019/2/19 下午12:35:55] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
[2019/2/19 下午12:35:55] [INFO] Cortex_R4_0: Instance deinitialized!
4. and when i return to the sdk demo'bin in above 2, i got the same problem, it seem that the vital sign lab's bin caused the com port com3 's problem.