Other Parts Discussed in Thread: AWR1642BOOST-ODS, IWR6843, AWR1642BOOST
I have a deployment requirement where IWR 1642 has to be mounted indoors on a ceiling facing down (maximum range is 10m). It needs to detect,classify and track objects in its field of view. The velocity of the objects will not be more than 10 Kmph.
As IWR1642BOOST antenna pattern doesn't measure elevation, I understand when the board is mounted top down, resolution on one axis of X,Y plane is lost.
This is confirmed in this thread
However I also found a thread where by re positioning one of the Tx antenna's elevation can be measured. If simultaneous measurement of elevation and azimuth is as simple as depicted in this thread, Why is the IWR1642BOOST not having such an antenna pattern?. What will be the trade off if the Tx antenna's are positioned as per the below thread?.
Will this antenna pattern be sufficient enough for my use case of 10m range and 10Kmph velocity? For the use case, the required minimum object separation resolution is 15cm on the XY plane. Can it be achieved.