Other Parts Discussed in Thread: UNIFLASH, , MMWAVEICBOOST, IWR1642, IWR6843
Tool/software: Code Composer Studio
Hi there,
I have a IWR6843ISK with MMWAVEICBOOST mmWave sensors carrier card and I managed to successfully flash the firmware of people counting demos for lab15 and lab19 using Uniflash:
C:\ti\mmwave_industrial_toolbox_3_1_1\labs\lab0015_pplcount_68xx\quickstart\PC_lab_xwr68xx.bin
C:\ti\mmwave_industrial_toolbox_3_1_1\labs\lab0019_pplcount_long_range_68xx\quickstart\LRPC_lab_xwr8xx.bin
Uniflash says the successful download.
However, after removing jumper SOP2 and reset the board and running the corresponding pplcount_gui.exe I am getting the following error after pressing start:
dfeDataOutputMode 1
channelCfg 15 5 0
adcCfg 2 1
adcbufCfg 0 1 1 1
profileCfg 0 61.00 35 6 43.0 0 0 8.241 1 125 3433 0 0 48
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
frameCfg 0 1 128 0 50 1 0
lowPower 0 0
guiMonitor 1 1 0 0
cfarCfg 4 4 4 16 16 4 4 50 50 0 1
doaCfg 1 1 1047 3 600 10 100
SceneryParam -15 15 0.5 22
GatingParam 4 4 5 0
StateParam 4 10 60 60 20
AllocationParam 40 200 0.5 40 2 2
AccelerationParam 1 1 1
trackingCfg 1 2 250 20 78 121 50 90
compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
sensorStart
Error 0x16 at ../src/termios.c(512): The device does not recognize the command.Error 0x16 at ../src/termios.c(2723): The device does not recognize the command
Error 0x16 at ../src/termios.c(512): The device does not recognize the command.Error 0x16 at ../src/termios.c(512): The device does not recognize the command.
Error 0x16 at ../src/termios.c(2723): The device does not recognize the commandError 0x16 at ../src/termios.c(2723): The device does not recognize the command
Error 0x16 at ../src/termios.c(512): The device does not recognize the command.Error 0x16 at ../src/termios.c(512): The device does not recognize the command.
Any help on that please
Thanks
Amin