This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Boost board setup to use FT4232 in place of XDS110 for com ports

Part Number: IWR6843ISK

To test the 50m people counting demo using the FTDI FT4232 on the boost board as the 2 com port source in place of the XDS110 I changed the board switches per the attached doc.  Is this the proper procedure?  The application did not run with these settings. It could be the software is not setup to adjust the FT4232 to the proper baud rates for the com ports.

Changing the IWR6843 Com from the XDS110 to the FTDI FT4232.docx