This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA970EVM: Unable to generate a sine wave on primary coil

Part Number: PGA970EVM
Other Parts Discussed in Thread: PGA970

Hi, I'm using the PGA970 EVM board through the GUI and it looks like the PC and and PGA are communicating, but I'm having trouble generating a sine wave on my primary LVDT coil. Looking for a 5 kHz sine, and this is what I'm getting scoping TP70 (red) and 71 (blue), this sawtooth form, @ 445 Hz between cursors. I get this regardless of having the LVDT connected or not. TP measurements as follows, GUI settings per screenshot... 

T3 = 7.488V

T2 = 4.958V

T4 = 3.295V

TP3 = 1.847V

TP6 = 2.995V