This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AWR1642BOOST: Running SRR Demo (TIDEP - 0092) without opening the GUI

Part Number: AWR1642BOOST


Tool/software: Code Composer Studio

Hi all,

I have the same question as the thread : http://e2e.ti.com/support/sensors/f/1023/p/727721/2689279 I would like to run the SRR demo without Matlab GUI

the last answer in the above thread says there is a "UART_read()" in "CLI_task()" in file "mmwave-sdk-install\ti\utils\cli\src\cli.c" 

but I can't find where the SRR demo code uses the CLI_task() or UART_read() function.

I wonder where should I bypass the CLI (CLI_task) and then call the AdvanceframeCfg and sensorstart functions

hope you can help me figure this out, thanks a lot!!

BR

Brian