Hello,
I am using the TDC1000-TDC2700EVM and want to use a external function generator, to ensure i can excite my ultrasonic transducers at a variety of different frequencies.
The setup was as following:
- the external function generator was connected to the input on the board designated for external clock (sine wave @ 1.6MHz, U(peak to peak) = 5V)
- JP6 jumper was moved to the EXT position
- On setup page of GUI set:
TDC_CLK_SOURCE_SEL to EXT_CLK
CLKFREQ(1-16MHz) to 1.600000- for 1.6MHz as source input.
- On TDC1000 tab
set the divider to 8 (1.6MHz/8 = 200kHz)
- Turned on the continuous trigger mode and couldnt see anything on my scope, probing the TX path.
Any suggestions on what could be wrong at my setup?
Thanks in advance and best regards.