Other Parts Discussed in Thread: IWR1642, , TIDEP-0094, IWR1443, IWR1443BOOST
Hello.
I did several tests with several of the available configurations and with different parameters of the MMWave Demo Visualizer, v 3.0.1 and IWR1642BOOST. evaluation board with a person moving before the radar in the range 10-30m. To make detection easier I used a flat aluminum table with size 70x50 cm hold vertically directly in front of the radar (so horizontally there is a 0.5m object size). All results was that after 20-25 meters the detection point becomes very unstable, so the max. realistic range of IWR1642 is 25m. But the Max Unambiguous Range [m] in the Visualizer is set to 50m, and Range Resolution is 0.1 m (Best Range option). Is this result expected? According to www.ti.com/.../tidud93.pdf there should be possible to detect objects with 0.3 m size up to 80 m. Is this hardware limitation of the EVM? How can I reproduce the 0.3 m objects detection at 50 m with the Demo Visualizer?
Thanks.