This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-TDC7200EVM: interfacing of ultrasonic sensor with TDC1000- TDC7200 EVM

Part Number: TDC1000-TDC7200EVM

I want to install ultrasonic transducer on the top inside of the tank for diesel level measurement in Generator Tank. The application is to measure the level through air medium along the X-axis.

The tank dimensions are as follows:
1) 1200 * 900*900 mm^3
2) 1828*1706*252 mm^3

I have gone through the following two transducer specifications and found them suitable to interface with TDC1000- 7200 EVM module. Kindly have a look and revert back with your feeback.

Also if you could suggest with a better transducer, kindly let me know.

1) www.audiowell.com/.../product-detail.aspx
2) www.steminc.com/.../piezo-ceramic-disc-10x2mm-r-215-khz-wire-leads-smd10t2r111wl