Part Number: TDC1000-TDC7200EVM
Dear TI Team,
The SteMinc team has suggested to use SMD50T21F1000R https://www.steminc.com/PZT/en/piezo-electric-disc-50x21mm-r-1-mhz ultrasonic sensor for measuring tanks having height 90cm. However, I need the parameters to feed into the TDC1000 to make it work with this disc either in axial or radial mode. I have already referred the technical notes in which the implementation of SMD10T2R111 is explained but could not find a solution for the above stated application
Kindly do the needful so that I can move ahead with testing of the evaluation module. If needed , I am ready to provide the samples of SMD50T21F1000R.
Thanking You,
Nikita Pal