Hi everyone!
I make the radar on the IWR1642 ICs. I program the next chirp parameters (see image#1):
Frequency start: 1425452105 (76.49546177 GHz);
Idle Time: 400 (4 usec);
TX Start Time: -400 (-4 usec);
ADC Valid Start Time: 200 (2 usec);
ADC Sampling Time: 2 usec;
Ramp End Time: 6 usec;
tsr: 0.25 usec;
BWsw: 4 MHz.
Image#2 shows a downconversion chirp frequency vs time. It is seen that in the working area saw nonlinear. My application is sensitive to this. How can a saw be made more linear? Increasing the guard intervals does not correct the situation.