Other Parts Discussed in Thread: UNIFLASH, , MMWAVEICBOOST
I'm trying to get started with the IWR6843ISK + MMWAVEICBOOST kit but when I try to flash the bin through Uniflash I receive a COM Port permissions error. I've attempted to do this on Mac and PC (Bootcamp and Native). My settings are listed below. Any assistance would be appreciated.
mmWave SDK 3.2
Windows 10
Power 5V 3A
Using provided USB Cable (But other USB cables fail the same way)
Uniflash Cloud/Offline v5/Command Line
IWR6843isk + MMWAVEICBOOST
SOP0 1
SOP1 0
SOP2 1 (Closed)
S1.1 0 (Off)
S1.2 1
S1.3 1
S1.4 1
S1.5 1
S1.6 1
S1.7 1
S1.8 0
S1.9 0
S1.10 1
S1.11 1
S1.12 1
USB Connected to XDS110-USB
Pressed SW2 (NRST)
DS1 Amber
DS2 Amber
3V3 Green
[LED Bank]
5V Red
NERR Off
3V3 Red
SOP2_FT Amber/Green
SOP1_FT Off
SOP0_FT Amber/Green
NRST Red
Attempting to flash xwr68xx_mmw_demo.bin
Image Loading Failed: Not able to connect to serial port. Recheck COM port selected and/or permissions.
Cortex_R4_0: Connecting to COM Port COM10…
Cortex_R4_0: Reset connection to device
Cortex_R4_0: Set break signal
[ERROR] Cortex_R4_0: Initial response from the device was not received. Please power cycle device before refreshing.
[ERROR] Cortex_R4_0: Not able to connect to serial port. Recheck COM port selected and/or permissions.