hello ,
To cover 1 km of distance by using sampling frequency 250 MHz , what should be slope rate and IF bandwidth . Please guide me with smart explanation (with equations), your all response is very valuable for me .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello ,
To cover 1 km of distance by using sampling frequency 250 MHz , what should be slope rate and IF bandwidth . Please guide me with smart explanation (with equations), your all response is very valuable for me .
Naveen,
TI has not tested the AWR1642BOOST EVM in a standalone radar sensor configuration for a 1 km range. The maximum range TI has tested is about 120 meters which can be seen in our Short Range Radar (SRR) lab found in the automotive toolbox in TI's Resource Explorer.
This sensor does not support a sampling frequency of 250 MHz. The max IF bandwidth is specified in this whitepaper: http://www.ti.com/lit/an/swra553/swra553.pdf
You can also use the mmWave Sensing Estimator Tool to determine your chirp configurations. It appears that a 1 km range is theoretically possible but this kind of chirp profile has not been tested.
Regards,
Kyle
Respected ,
I understood the point that you made, but there is some issues related to calculation. As in the tutorials of TI telling that the chirp is having sweep bandwidth of 4GHz in 40us which corresponds to slope of 100MHz/1us. By this when i was trying to calculate IF frequency by using formula IF_frequency = (slope *2*range) /c , where range is 120 mts . After calculating , IF frequency = 80 MHz which is greater than the 5MHz ( IF bandwidth ). You suggested me to calculate chirp parameters by below link
https://dev.ti.com/gallery/view/1792614/mmWaveSensingEstimator/ver/1.3.0/
I tried to calculate, where it is showing bandwidth 370.55 MHz and chirp repetition time 54us which corresponds to slope of 6.8519 MHz/ 1us. when i calculated IF frequency with this values i got 5.23 MHz . if this is correct tell me that how can it give 4 cm range resolution which is written in all documents that TI have, with 370.55 MHz it is only possible to give 40 cm not 4 cm . Please clear my doubt as quick as possible .Thank you.
The computation of range resolution has been extensively discussed in the forum.
Please see
http://e2e.ti.com/support/sensors/f/1023/t/792204?IWR6843-Range-resolution-of-this-device-
Naveen,
Please refer back to the whitepaper that I listed in my previous post to find more information about how we arrive at a best range resolution of 4 cm.
Regards,
Kyle