Hi Team,
Here is another question about the EEPROM programming problem in PGA460. When customer sends order "0" (55 00 01 fe), the PGA460 doesn't respond, and the code in EEPROM doesn't run. Customer measures the voltage of OUTA and OUTB is high, and customer read DEV_STATO register (55 09 4ca a) get feedback number (40 84 3B).
Do you have any suggestions to this phenomenon ?
By the way, can the PGA460 measure ultrasonic wave whose frequency is between 30 and 500 KHz ? If not, can you recommend one device to me ?
Many thanks~
Stanley Dai