This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to run mmwavelink_example.exe

Part Number: AWR1243BOOST


I have an AWR1243BOOST connected to a DCA1000. All devices are showing up correctly in Windows. I can run mmWave Studio and connect successfully. However, when I try to run the examples in the DFP I cannot. When I run mmwavelink_example.exe I get the following output:

(base) C:\ti\mmwave_dfp_01_02_00_01\ti\example\mmwavelink_example>mmwavelink_exa
mple.exe
=========== mmWaveLink Example Application ===========
rlComIfOpen Callback Called for Device Index [0]
Got 4 devices connected
Device 0: AR-DevPack-EVM-012 A , SN: FT3E75YSA
Device 1: AR-DevPack-EVM-012 B , SN: FT3E75YSB
Device 2: AR-DevPack-EVM-012 C , SN: FT3E75YSC
Device 3: AR-DevPack-EVM-012 D , SN: FT3E75YSD
SPI port opened (PortNum=0)
IRQ & I2C port opened (PortNum=1)
Board Control port opened (PortNum=2)
Generic GPIO port opened (PortNum=3)
rlDeviceEnable Callback is called by mmWaveLink for Device Index [0]
mmWave Device Power on failed for deviceMap 1 with error -8

=========== mmWaveLink Example Application execution Failed ===========

Any idea what's going wrong? Thanks in advance.