Other Parts Discussed in Thread: DRV401,
I have the following questions about fluxgate current sensor modulation chip, please refer to, thank you!
1, the following figure "parameter list" DRV401 can be applied to 1A primary rated current Ipn, how to change the value of peripheral resistance Rshunt to detect 1A current? Taking 1A as an example, how to calculate the resistance value of Rshunt? What is the current range that DRV401 can test?
2, how to determine the primary current range that can be detected from the parameters of the modulation chip data manual?
3, why is the ERROR pin in the chip connected to the Vout pin?
4, according to the data manual, the over-range pin should be raised, but why can the over-range pin be suspended in the application circuit?
5, the REFin pin is connected in series with a resistance to the REFout pin. Must the sum of resistance in series be 4 times Rshunt resistance?
6, according to the data manual, the gain of the chip is 4. How can the gain of 1.2V/A be realized by changing the resistance value of the peripheral circuit?
7, why do some circuits connect the / PWM (19PIN) pin to the R-C-R (T filter) and then connect the series capacitance C to the IAin2 pin? And some application circuits put the pin empty?
1.docx8, the following is the product Ipn=1A chip application structure diagram, compared with the DRV401 application example is consistent, but compared with the DRV421 application diagram is inconsistent, the DRV421 application routine connection is two red circle connection exchange, what is the reason why the two chips are inconsistent in the red circle position connection?