Other Parts Discussed in Thread: IWR1443BOOST, MMWAVE-SDK
In the post entitled "RTOS/IWR1443BOOST: ISSUE Flashing IWR1443Boost", John H gave steps to convert the High Accuracy project from supporting the ES2 to the ES3 hardware. He said to compare the changes in the projectspec file between two versions of the OOB demo lab and make those changes to the high accuracy lab file. It further states to compare the demo source code and then make the same type of changes to the High Accuracy lab files.
There are differences in the r4f_linker.cmd files. Do those need to be incorporated? Trying to do so yields build errors because some of the length macros are not defined in the High Accuracy lab. It is not apparent where the macros are defined.
Left unanswered from the above post was what to do with the .h files that don't appear in the newer demo lab. Should those files be taken out of the High Accuracy lab?
Some more explicit description of the required changes would be appreciated. Even better would be that the High Accuracy lab be updated by TI for use with the ES3 hardware.
Partway through the above post, there was mention that focus has been taken away from the High Accuracy lab. Is that true? Is there another lab that works with the ES3 hardware and that will provide high accuracy distance measurements?
Alan