This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Minimum distance from sensor for the range resolution

Part Number: IWR6843

Hi,

I understand that range resolution is the minimum distance between two objects to be detected separately. 

However, I wanted to know at what distance from the sensor is range resolution valid?

I mean can I put two objects 3.75 cm apart at any distance e.g. 0.5 or 1 meter distance from sensor and they will still be detected as different or is there is something more to it?

Thank you.