This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Information flash usecase: Save user data to QSPI flash and backup

Part Number: AWR1642

Hello team,

Customer plan to use a sector in QSPI FLASH to save the user information. They plan to use 2 sector, one is for backup.

The only thing that need to be concern is. If the power of device is drop when writing data to qspi-flash. Then the device should goto backup area to read the user configuration at next boot.

Do we have any reference design/code to read/write the QSPI flash like this way?

Thanks,

Wesley