This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: can not find the DCA1000

Part Number: DCA1000EVM


when I use mmwave Studio to connect the DCA1000,it can not find the COM port?what should i do to solve it.Thanks.

  • Hi,

    Please make sure you have a USB cable connected to the "RADAR_FTDI" USB port of the DCA1000 EVM. Also ensure that you have the FTDI drivers installed and that you see the FTDI ports show up in device manager.

    The drivers are available here: 

    Please also ensure that the DCA1000 is separately powered.

    Best Regards,

    Anand