While going through processor requirements for opt8320 sensor specified by ti,it was noticed that the capabilities mentioned are cortex m4 running at 200mhz or cortex a9 running at 800MHz or A15 running at 1.5GHz is suggested.Why is that so? Can a processor of M4 series running at 180Mz meet the requirement of the same.